We have an softstarter ATS48C48Q that is displaying the OCF code. We have been following the instruction on User´s Manual : checking the motor and wir...

Goals and Symptoms

We have an softstarter ATS48C48Q that is displaying the OCF code. We have been following the instruction on User´s Manual : checking the motor and wire isolation, by-pass circuits testing, and the others instrucctions. We didn´t find anything that explains the situation. The OCF code is displayed randomly, in anytime, inclusive without the RUN command actived and without the power supply L1-L2-L3 conected. Could you say us what antohers causes are posible? We already have changed the control board, but the result is the same : the OCF code continues diplaying.

Facts and Changes

OCF

Causes and Fixes

Try to replace the power board because a bad solding is also possible, or the best way is to replace the complet product.


Legacy KB System (APS) Data: RESL156439 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: