Søg i ofte stillede spørgsmål
What are the various NIM (Network Interface Module) models available for Advantys?
The following table shows the various Advantys NIM models:
NOTE: All of the Basic NIM's are obsolete and will need to use the standard NIM's.
Fieldbus | Part Number | Description |
Profibus DP | STBNDP2212 | Profibus DP standard NIM |
STBNDP1010 | Profibus DP basic NIM | |
INTERBUS | STBNIB2212 | INTERBUS standard NIM |
STBNIB1010 | INTERBUS basic NIM | |
CANopen | STBNCO2212 | CANopen standard NIM |
STBNCO1010 | CANopen basic NIM | |
DeviceNet | STBNDN2212 | DeviceNet standard NIM |
STBNDN1010 | DeviceNet basic NIM | |
Ethernet | STBNIP2212 | Ethernet MB TCP/IP standard NIM |
Modbus Plus | STBNMP2212 | Modbus Plus standard NIM |
Fipio | STBNFP2212 | Fipio standard NIM |
Udgivet til:Schneider Electric Danmark
Se mere
Område:
Se mere
Område: