STBNIP2212 Advantys Ethernet NIM Gateway Configuration

Goals and Symptoms

When configuring an Advantys STBNIP2212, a gateway address with the last octet of x.x.x.255 cannot be used.

Causes and Fixes

Users must avoid using x.x.x.255 as a gateway address with the STBNIP2212.
If x.x.x.255 is required to be used as the gateway address, then the STBNIP2311 should be considered.


Legacy KB System (APS) Data: RESL203940 V1.0, Originally authored by RiCr on 11/19/2010, Last Edited by RiCr on 11/19/2010
Related ranges: Modicon STB

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: