Søg i ofte stillede spørgsmål
What does Error Code 11 (hex B) indicate on a READ_VAR using the M340 native ethernet port?
Error Code 11 ( hex B ) is defined as "No processor system resources". What this means is that the M340s ethernet port is not available to process the message. This could be due to a full buffer or no sockets available. One possible solution is to cycle power to the PLC to clear the buffer. Adding a time out value to the GEST parameter can minimize the frequency of this message.
Legacy KB System (APS) Data: RESL212290 V1.0, Originally authored by DaSo on 08/12/2013, Last Edited by DaSo on 08/12/2013
Related ranges: Modicon M340
Udgivet til:Schneider Electric Danmark
Se mere
Område:
Se mere
Område: