Søg i ofte stillede spørgsmål
How do the program and data get stored in the memory of Quantum PLC
In case no memory extension card is used with PLC, then the program data and constants are stored in the internal RAM memory of the processor module only.
However, when the memory extension card is used with PLC, then data is stored in the internal RAM memory of processor module, whereas programs and constants are stored in the memory extension card.
Udgivet til:Schneider Electric Danmark
Se mere
Område:
Se mere
Område: