Do the PM800 series I/O modules work with the PM810?

Issue:
Do the PM800 series I/O modules work with the PM810?

Product Line:
PM810
PM8M2222
PM8M22
PM8M26

Cause:
Customer would like to know whether the PM800 series I/O modules work with the PM810.

Environment:
Compatibility between PM800 series I/O modules with PM810.

Resolution:
Any of the PM800 I/O modules will work with a PM810 with firmware 10.2 and greater.

For more information about upgrading firmware please visit https://www.se.com/ww/en/faqs/FA237920/

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: