What is the maximum number of simultaneous IEC6150 and Modbus TCP open connections supported by the G3200?
Issue
Unable to connect to the G3200 gateway

Product Line
G3200

Resolution
The G3200 supports up to 6 simultaneous IEC61850 and 4 Modbus TCP/IP connections at one time. If this maximum number of connections is met, no other connections are allowed to the device.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: