Søg i ofte stillede spørgsmål
How can I use PID controls on an E-Flex or M-Flex that has an HOA switch?
Issue:
Trying to setup PID control on an ATV61/71 with a HOA switch.
Product Line:
ATV61/71, E-Flex, M-Flex
Environment:
All of the ATV61/71, E-Flex, M-Flex
Cause:
None
Resolution:
To allow PID control in Auto mode and manual reference control in HAND, the logic input for PID AUTO/MAN or reference 2 switch must be setup so that the contact is closed in HAND mode and open in AUTO mode. The logic input causes the manual control to override the PID.
Udgivet til:Schneider Electric Danmark
Se mere
Område:
Se mere
Område: