Does Unity Pro include state ram when importing a ProWORX project?
Issue
When opening/importing a ProWORX project which included State ram into Unity Pro, is the state ram included?
Product Line
Unity Pro, ProWORX
Resolution
Yes. State ram addresses are brought into Unity Pro as variables. The naming syntax is as follows:
400001 would be seen in the Unity Pro Variable Editor as _400001 located to %MW1.
000001 would be seen as _00001 located to %M1.
100001 would be seen as _10001 located to %I1.
300001 would be seen as _30001 located to %IW1.
These values can be seen online to the CPU or the simulator by displaying them in the Animation Table.

***If you do not see the state ram values after loading the Unity Project, make sure that 'Initialize %MWi' is checked on the CPU configuration page before transferring the project.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: