Is "remote reset" function available for GV2 / GV3 / GV4 / GV5 / GV7 circuit breakers?
There is no remote reset available for any of the GV range circuit breakers; GV2, GV3, GV4, GV5, GV6 nor GV7. Remote tripping using a shunt trip or undervoltage release is possible but there is no remote reset. Note that the GV7 range is obsolete, replaced by GV4/GV5.

Auto reclosers are available for the iC60 range - enter 'ARA auto recloser' into the search bar on www.se.com/uk to find this range.

ComPact NSX & Masterpact breakers have optional or native remote reset mechanisms, depending on the part number.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: