Video: Resetting a LTMR Tesys T module back to factory default settings locally
Issue :
How to reset a LTMR Tesys T module back to factory default settings locally?

Product Line:
Motor control / Protection components

Environment:
LTMR
Tesys T

Cause:
Need to reset the module back to factory default settings locally to clear any user configuration.

Resolution:



1) Make sure the module is in one of the following states : Ready, Not ready or System configuration. (If the product is in Start or Run state, the return to factory setting is ignored)
2) Press and hold the Test/Reset button down for more than 15 seconds , but not exceeding 20 seconds and release it.
3) The unit will execute a reset to factory settings.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: