What are the part numbers of the replacement power contacts for TeSys F contactors?

Please note - The TeSys F range is now obsolete, the information below is for reference only. TeSys F was replaced by TeSys Giga, you can find details of this range here - TeSys Giga | Schneider Electric UK (se.com)

Spare parts required for each pole of LC1F*** contactors are as follows:

  • 2 fixed contacts
  • 1 moving contact
  • 2 deflectors
  • 1 backplate
  • Locking screws and washers

These parts are supplied in complete sets of contacts for each contactor size and are dependent on the number of poles per contactor.

An example of contact set part numbers would be LA5FG431LA5FG431

Part numbers for complete packs of contact sets for LC1F contactors are attached below:


Sets of Contacts

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: