Is there a replacement for Schneider Electric's ATVPOT25K speed potentiometer for Altivar drives?

Article available in these languages: Spansk

Issue:
ATVPOT25K  speed potentiometer obsolete replacement  for Altivar drives

Product Line:
Altivar Machines

Environment:
All models and serial numbers

Cause:
Selection of Speed Potentiometer for speed control

Resolution:
Altivar VFD's can use a speed potentiometer from 5K ohms to 10K ohms.

Suggest using one of the following:
For 22mm
Metal - XB4BD912R10K
Plastic - XB5AD912R10K

For 30mm
Metal - 9001K2108
Plastic - 9001SK2108

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: