Can I display database timestamps as Local Time rather than UTC?
Issue
The timestamps in the ION_Data database are stored in Universal Coordinated Time (UTC). A user would like to show these timestamps as Local Time.

Product Line
PME 8.x, 9.0, 2020, 2021, 2022, 2023
Power Monitoring Expert 7.2.x
StuxureWare Power Monitoring 7.0.x

Environment
SQL Server Management Studio

Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by
users familiar with SQL Server Management Studio. Databases should be backed up before
performing this procedure.*


This article describes a simple workaround to display the timestamp in local time instead of UTC. The DATEADD() function adds or subtracts a specified time interval from a date when executing a SQL query.

The following SQL query utilizes the DATEADD function to convert from UTC to Pacific time ( UTC -8) and creates a new temporary column ' local time that displays the corresponding result:

SELECT TOP 1000 [ID]
,[Value]
,[SourceID]
,[QuantityID]
,DATEADD (HH,-8,TimestampUTC) as LocalTime
FROM [ION_Data].[dbo].[DataLog2] order by LocalTime desc


The '-8' corresponds to Pacific Time (UTC -8) and will need to be changed to convert to other time zones. The figures below show Executed query results as well as the original query :

SQL Query Result
Another example :
SQL Query Result SQL Query Result




Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: