Where can I get a part number for the temperature sensor on the Walmart system units racks?
Issue:
Where can I get a part number for the temperature sensor on the Walmart system units racks?

Product Line:
Altivar ATV61 Eflex Walmart units only

Environment:
Walmart location Drives only

Cause:
They need a replacement rack sensor.

Resolution:
They need a replacement rack sensor which is not part of the Schneider Electric drive. You will need to go back thru the Novar or Emerson supplier to get these parts.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: