%MW49..53 seem to be in UTC, how can I get the local time ?
In M580, the words %MW49..53 are in UTC (Coordinated Universal Time), and not in local time.

If local time is needed, use the function RRTC_DT
(note that RRTC_DT_MS is also in UTC time)

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: