Why is it when I do an export in Vijeo Designer, it saves the project file type as a .HMIX?
When exporting a target in a project, it can only save the type as a .HMIX. When exporting an entire project, it must be done in the Vijeo Manager which will export the project as a .VDZ archive.