How can I order NEMA style contactors with Enclosed ATS48 soft starts?
Issue:
Order NEMA style contactors for the Enclosed ATS48 soft starts.

Product line:
Enclosed ATS48, Class 8639, Type 48U.

Environment:
All

Cause:
Option not shown in the Product Selector tool.

Resolution:
You must choose Mod W10 which includes  NEMA Style contactors   Please note this option is not available on the Power Circuit R reversing or Mod A10 full voltage bypass option.

Schneider Electric Danmark

Bilag
30072-450-62_02.pdf [1.93 MB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: