Can the NetShelter SV be joined with other ISX Row Based components (InRow Cooling, UPS, PDUs)?
Issue:
Customers want to use the NetShelter SV in an ISX Row Based architecture with other cabinets, InRow cooling or PDUs.

Product Line:
NetShelter SV

Environment:
All versions and serial ranges.

Cause:
Customers want to align the SV to adjacent cabinets using the baying brackets.

Resolution:
The NetShelter SV is not optimized for ISX Row based architecture. The SV frame does include baying brackets and joining holes for alignment and joining to adjacent cabinets but alignment may be difficult due to the different height, depth and frame design of the NetShelter SV, SX and VX cabinets. Height adapters are not available for matching the height of the NetShelter SV to ISX components.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: