What is the default IP address of an ACE850TP/ACE850?
Issue
A user would like to know the default IP address, subnet mask and gateway information for an ACE850TP/ACE850

Product Line
ACE850TP/ACE850

Environment
Sepam/ACE communications

Cause
Default parameters for the ACE device needed for communication

Resolution
The default parameters for the ACE850/ACE850TP are:
IP Address169.254.0.10
Subnet Mask255.255.0.0
Default Gateway0.0.0.0

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: