Where are the DC bus connections on a ATV61 drive?
Issue:
Looking for the DC bus connections on a ATV61 Drive.

Product Line:
All ATV61 drives

Environment:
All

Cause:
N/A

Resolution:
The DC connections are at PA/+ and PC/-.  These are located with other power terminals L1L2L3 and T1T2T3 or at the top near the DC choke.  See the attached files for installation manual information.

Schneider Electric Danmark

Bilag
ATV61 Low HP installation manual.pdf [2.38 MB]
ATV61 High HP installation manual.pdf [4.58 MB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: