what are the OIDs for reading the port link status from Connexium Ethernet Switch TCSESM083F23F1 using SNMP Protocol in a MIB browser.
Issue:

Customer wants to use SNMP protocol to read port status of the ethernet switch

Product Line

Connexium Ethernet Switch TCSESM083F23F1

Environment:

Windows 7 Pro

Resolution:



The very first step is to install the correct MIB file in the MIB Browser.
We need to install the two files in the MIB Browser.

1.SchneiderTFE-V03-00.mib
2.SchneiderElectricSwitches_V02_00.mib.
Contact your local country Schneider Electric Customer Care Center to get this files.

The port status can be up(1), down (2).
The OID for reading the port status is read as below.
Port x >>  oid=".1.3.6.1.2.1.2.2.1.8.x"

Where "x" denotes the number of port in the switch.





Schneider Electric Danmark

Bilag
Port Status and LED Status.xml [2.39 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: