How to completely remove Vijeo Designer Runtime from a PC
Issue
How does one completely remove Vijeo Designer Runtime from a PC?

Product Line
Vijeo Designer Runtime
VJDSNRTMPC
VJDSNRTSPC
VJDRPCCZLSPMZZ
VJDRPCCZLSPAZZ
VJDHPCCZLSPMZZ
VJDHPCCZLSPAZZ

Environment
HMI Runtime software for Windows PC

Resolution
To bring the PC to a state with Vijeo Designer Runtime completely removed, there are two methods available.

Method 1 (the Windows Uninstaller Method):
Uninstall Vijeo Designer Runtime from Windows "Add/Remove Programs". Looking for Vijeo Runtime and then choose Uninstall.

Method 2 (Deletion of Files):
1) Delete the folder and the contents of the folder:
C:\Program Files (x86)\Schneider Electric\Vijeo-Designer\Vijeo-Runtime\
(on older 32bit Windows PCs):
C:\Program Files\Schneider Electric\Vijeo-Designer\Vijeo-Runtime\

2) From the folder "C:\Windows\", delete the file named "57340"

3) Delete the Registry folders (if they exist):
Computer\HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Schneider Electric\Vijeo-Designer\
Computer\HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Schneider Electric\Vijeo-Designer Runtime\
Computer\HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Schneider Electric\Vijeo-Designer-Runtime-PC-V2020 (this folder exists for 6.2 SP11+)


(on older 32bit Windows PCs):
Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\Vijeo-Designer\
Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\Vijeo-Designer Runtime\

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: