Can ATV312 drive display RPM instead of Frequency?
Issue:
How to display the RPM on an ATV312?

Product Line:
ATV312

Environment:
All model numbers, all serial numbers

Cause:
Customer wants to display the RPM on the drive display.

Resolution:
This can be done by creating custom display parameter.
In menu SEt-, go to SdS and set it to RPM/60Hz then press enter to save it.
Go back to menu SUP and go to SPd3, press enter twice to set it.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: