Video: How do you configure the sink and source switch on the Altivar ATV312 drives?
Issue:
Setup the sink and source switch on the ATV312 drives

Product Line:
Altivar ATV312

Environment:
All

Cause:
Needs to check to see what position the sink source switch is in.

Resolution:
You can check the sink source switch position by checking to see what position the sink source switch is set to on the printed circuit board of the ATV312 drive.


Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: