Søg i ofte stillede spørgsmål
How do you adjust the pressure on an XMLA, XMLB or XMLC pressure switch without a display?
When the product does not have a display, we recommend using a pressure gauge to set the increasing pressure.
The pressure is adjusted by means of the adjusting screw located on top of the product. The image below shows an example of this.
![XMLA XMLA](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H0000088ZFeQAM&oid=00DA0000000abSm)
The complete XML* setup manual is attached.
The pressure is adjusted by means of the adjusting screw located on top of the product. The image below shows an example of this.
The complete XML* setup manual is attached.
Udgivet til:Schneider Electric Danmark
Bilag
Se mere
Område:
Se mere
Område: