What can I do if the PLC TM221 reboots continuously after an update with firmware 1.3.2.1 SP1?
Article available in these languages:Japansk
This issue can be solved by downloading any application in the PLC TM221 via USB in powerless mode (no power supply connected). After that, the issue will not appear anymore.