What is the replacement for the XBTGT7340?
Issue:
What is the replacement for the XBTGT7340?

Product Line:
Magelis HMI, XBTGT7000 series

Resolution:
The replacement for the XBTGT7340 is the:

HMIG3U + HMIDT732 display (if video playback is not needed)
HMIG5U2 + HMIDT732 display (if video playback is needed)

Vijeo Designer V6.2 SP3.1 or greater is required for the HMIG3U / HMIG5U
Vijeo Designer V6.2 SP7 or greater is required for the HMIG5U2

Schneider Electric Danmark

Bilag
Transition Tool for XBTGT7340.pdf [757.12 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: