If the customer wants to change the bridge with keeping its Remote, is it enough to switch it OFF and then to switch it ON in order to find the Base linked to the other bridge he wants to drive. Is it right ?
If using a display remote device, a long reset (>5s) is enough.If using a LED remote device, the configuration SW is mandatory.