If the operator use eXLhoist in a driver room (like use joystick), and the distance is nearly 15 meters, is this ok to use ?
We made some tests here and 15 meters should be not a problem. Anyway it depends on the material of the separation between the driver room and the Base. The external antenna can be used in order to reassure the customer.