What are the part numbers for the RJ45 Modbus cables for Schneider drives and soft starters?
VW3A8306R03 -  0.3 meter length cable / 1 foot
VW3A8306R10 - 1 meter length cable / 3 feet
VW3A8306R30 - 3 meter length cable / 9 feet

NOTE:  These cables will not work for connecting a remote mounted keypad for the drives/softstarts.
The best cables for remote keypad connections are:
VW3A1104R10 - 1 meter long / 3 feet
VW3A1104R30 - 3 meters long / 9 feet
VW3A1104R50 - 5 meters long / 15 feet
VW3A1104R100 - 10 meters long / 30 feet

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Danmark

Se mere
Produkt:
Se mere
Produkt: