Is there a way to determine how large a PME 8.x database is expected to grow over a period of time?
Issue
When installing or upgrading to a new PME 8.x server, a user would like to know an estimate of database size growth in order to determine hard drive space on the server.

Product Line
Power Monitoring Expert 8.x

Environment
Power Monitoring Expert Estimated Database Growth Calculator

Resolution

The attached calculator will assist you in estimating the Database growth for PME 8.x.  It uses default logging profiles, so if there is a change in what a device is logging (Onboard or Software Based), that will need to be factored into the calculation.

Schneider Electric Danmark

Bilag
(PME8.1)(Calculator) Database Growth Calculator.xlsx [30.48 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: