How to read the IP address of a High end M580 CPU
Issue

Where is the M580 IP address located?

Product Line

BMEP585040, BMEP586040
Unity pro 11 and above.

Resolution

The IP address is located in two system words: %SW6 and %SW7.

%SW6 contains the two last octets of the IP address and %SW7 contains the two first octets.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: