Can the ATV212 drive be mounted inside a Nema 3R enclosure?
Issue:
Mounting an ATV212 drive in a Nema 3R enclosure.

Product Line:
ATV212

Environment:
All serial numbers for ATV212

Cause:
N/A

Resolution:
Yes.  The drive comes as an IP20 open style unit and can be mounted in any customized enclosure.
Please reference the attached installation manual for dimensions, weight, mounting tips, air flow, heat dissipation and more

Schneider Electric Danmark

Bilag
Install S1A53832_03 ATV212.pdf [5.67 MB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: