- Open Scadapack E Configurator.
- Connect to the SCADAPack E rPAC or RTU.
- Goto Transfer Menu then Select Remote Command Line. A Remote Command Line (Vitual Teminal) window will appear. See figure 1
- Under C:\> type status events then all DNP events generated will be displayed.