Is it possible to use mechanical interlock using cables for source changeover for MTZ/NW/NT breakers inside BlokSeT Switchboard?
Yes it is possible to use the mechanical interlock by cables for MTZ/NW/NT breakers inside the BlokSeT column.

Below is the procedure which needs to be followed to have this solution inside the BlokSeT.
  1. The U-channel of the column should be cut as shown. The dimension of material to be removed is 200 x 25 as shown below.


2. Masterpact catalog gives source changeover to assemble in different combinations.






Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: