5914 USB to Bluetooth Adapter Module OS Compatibility
  • OS compatibility: Windows 2000, Windows XP 32 and 64-bit, Windows Vista 32 and 64-bit

Installing the device on Windows 7

Most Belkin Bluetooth USB adapters install automatically without any extra software on Windows 7.  Simply plug the device into a spare USB Slot.  Windows 7 should automatically recognize the device and install the necessary drivers and software.

If you encounter any issue's with this then you can try installing the latest drivers from the chipset manufacturer - http://www.broadcom.com/support/bluetooth/update.php
Or see link below for more details:

http://www.belkin.com/us/support-article?articleNum=4901

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: