What is the time delay between detecting a motor overload fault, and when power is removed from the motor on an ATV61 series drive?
Issue:
ATV61 time delay between detecting a motor overload fault and motor stoppage

Product Line:
ATV61 /ATV71 series drives

Environment:
All models, All serial numbers

Cause:
Information not available in current literature.

Resolution:
The time delay between a detected motor overload fault, and remove of power from the motor is 250 microseconds.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: