What values are stored in the Primary, Secondary and Tertiary registers for each Accutech wireless field unit type?
Accutech wireless field units have registers for Primary, Secondary and Tertiary process values. Please note that not all field unit types use all three process output values.
Field UnitPrimarySecondaryTertiary
AP10Pressure (PSI)Not Used (N/A)Not Used (N/A)
AM10Ultrasound (0 to 255)Temperature (deg C)Not Used (N/A)
DP10/DP20Pressure - DPNot Used (N/A)Unit Code
-Orifice Flow - FlowNot Used (N/A)Unit Code
-Open Channel Flow - FlowNot Used (N/A)Unit Code
-Fluid LevelNot Used (N/A)Unit Code
FL10Top Level (Inches)Bottom Level (Inches)Temperature (deg F)
GL10Pressure (User Configured)Not Used (N/A)Unit Code
GP10Pressure (PSI)Not Used (N/A)Not Used (N/A)
AI10Analog Input 1 (mA)Analog Input 2 (mA)Not Used (N/A)
AV10Analog Input 1 (V)Analog Input (V)Not Used (N/A)
RT10Temperature (deg C)Not Used (N/A)Not Used (N/A)
SI10Switch 1 (Counts or State)Switch 2 (Counts or State)Not Used (N/A)
SL10Pressure (User configured)Not Used (N/A)Unit Code
TC10Temperature (deg C)Temperature (deg C)Not Used (N/A)
TM10Flow Rate (gallons/minute)Total Flow (gallons)Not Used (N/A)
VC10Pressure (PSI)Pulse Count on Switch 1Not Used (N/A)































In general, the units for each field unit are fixed, despite the fact that you can change the units being displayed on the field unit display or in Accutech Manager. The exceptions to this are the DP10/DP20, the GL10 and the SL10, which can be used to measure different values such as Flow, Level or Pressure.

Schneider Electric Danmark