ACF400 Spare parts break down
Issue:
ACF400 Spare parts break down

Product line:
ACF400, ACF115, ACF136

Environment:
Air Removal Unit

Cause:

Resolution:
Please call tech support at 1-888-695-6500 and hit option to three times to get to the cooling team to verify part numbers before ordering, as they may change.

ACF400 break down
This is the entire fan and power system.
ACF115          APC Rack Air Removal Unit SX Fan Assembly 100-240V 50/60 Hz (All 4 fans and Electronics module included)
ACF136          APC Rack Air Removal Unit SX 600mm Wide Frame
ACF126          Ducting Kit
W0M-7053     ASSY ARU GEN 2 ELECTRONICS MOD
W0M-7054     AIR REMOVAL UNIT G2 REPLACEMENT FAN MODULE
0J-0G-9233     GENERIC ANSI WWPV LCD DISPLAY
0J-0W2818A  Temperature Sensor (Optional)
AP9324           Beacon (Optional)

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: