How to determine the Over and Under Range Alarm Modbus Register on a Scadapack models 314, 334 and 357 using Telepace Studio?

The SCADAPack 334 with 5607 I/O module is comprised of four types of I/O channels, digital inputs, digital outputs, analog inputs, and analog outputs.

The digital input assignment provides twenty four I/O channels for the digital input data from the SCADAPack 5607 I/O Module hardware. The digital input registers are updated continuously with data read from the digital inputs.

The 5607 I/O Module provides sixteen external digital inputs. These are externally wetted inputs.

The module provides 8 internal digital inputs, which indicate if the corresponding analog input is in or out of range.

See Configuration Example below:

Schneider Electric Danmark