What is the maximum length of cable between two IO modules using Scadapack?

The recommendation is 6 ft ( 72 inches) Starting from the I2C bus port of the Controller Board or the 5103 power supply module.

For example using the Diagram below

Schneider Electric Danmark