What is the replacement part number for Lexium 05 drive bearing part number LXM05AD10M2?
Issue: Replacement

Product Line: Lexium 05A

Environment: None

Cause: Obsolescence

Resolution:
The corresponding part number to replace a LXM05AD10M2 will be a LXM32AU90M2 in terms of current rating. Lexium 05A is a CanOpen drive and hence the direct option is to use a CanOpen drive. Some configuration changes at the drive and changes in the PLC program are to be expected. It may be better to understand the application to determine if a LXM32MU90M2 (modular drive with a different fieldbus module) or a LXM32CU90M2 standalone drive is a better alternative.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: