What is the maximum number of Modbus/TCP slave device words for TM258 / LMC058 and TM241 / TM251 controllers in SoMachine or Machine Expert?
Starting with SoMachine 4.1 SP2 a new firmware version: 4.0.2.xx was delivered. In this new version the maximum size of words increased for Modbus TCP slave device: %IW 120 words - %QW 120 words (previously 40 input / 40 output words).

Notes:
- The above information is correct also for Machine Expert 1.x and 2.x
-  EcoStruxure Machine Expert supports M258 and LMC058 controllers starting with version 1.2.5. Previous version of EcoStruxure Machine Expert did not support them.
- EcoStruxure Machine Expert v2.0 does support M258 or LMC058 controllers anymore.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: