Failed to Connect to the SEPAM front face using the USB cable.
Issue
When trying to connect to the SEPAM using SFT2841 with the mini USB to USB (CCA784) it fails.

Product Line
SFT2841

Environment
Windows computer management

Cause
The driver for windows is not get install or cannot find it.

Resolution
Attached are the work around for the XP and Windows 7 operating systems.  If one as Windows 7 or above follow the Windows 7 pdf.

Schneider Electric Danmark

Bilag
Computer connection to sepam with USB front panel - WinXP.pdf [640.67 KB]
Computer connection to sepam with USB front panel-Win7.pdf [817.22 KB]
Se mere
Produkt:
Område:
Se mere
Produkt:
Område: