Is it possible to copy the data from Magelis/Harmony CF/SD card to the USB stick?
Issue:
Is it possible to copy the data from Magelis/Harmony CF/SD card to the USB stick?

Product Line:
Magelis/Harmony, XBTGK/GT/GC, HMIGTO, CopyData operation, CF card, SD card, Vijeo Designer

Resolution:
With the latest version of Vijeo Designer v6.2 or higher.  The CopyData operation of the switch can be used.  This will allow to copy runtime data files from CF/SD card to USB as long as the Runtime data location are set to Secondary Drive.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: