Can an encoder be used with the ATV600 Series Process Drives?
Issue:
ATV600 Series Process Drive encoder usage

Product Line:
ATV630 ATV650 ATV680 Process Drive

Environment:
All models and serial numbers

Cause:
None

Resolution:
The ATV600 series Process drives do not have the ability to be used with an encoder. The ATV900 series is designed for encoder option modules.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: