Connect a remote OPC client to ClearSCADA

Problem

Need to connect a remote OPC client to ClearSCADA and bypass DCOM.

Solution

This can be achieved by installing the Data Access component of ClearSCADA on the remote machine that hosts the OPC client. To install and configure the Data Access component follow the steps below:

1. Run the ClearSCADA Installer on the remote machine hosting the OPC client and select "Install ClearSCADA".

2. Select Custom installation and only install the Data Access component:

SCADA setup

3. You should now see the Configure Connections program if you click on the Windows Start button. If the program cannot be located in Windows Start menu, the program can be run directly from: C:\Program Files (x86)\Schneider Electric\ClearSCADA\ClientConfig.exe (on 64-bit machines) or C:\Program Files\Schneider Electric\ClearSCADA\ClientConfig.exe (on 32-bit machines)

Tree structure

4. Run the Configure Connections program and create a connection to the ClearSCADA server by specifying the IP address (or server name) of the ClearSCADA server in the Node Name field of the Node A tab and select OK to apply the changes:
Scada client

5. Your OPC Client should now see ClearSCADA OPC Server among its local OPC servers as below:

Properties

The OPC service name appears in the following format based on the information defined within the Configure Connections program:

Serck.ScxV6OPC[OPC type].[System name].[Host address or IP address]

The Data Access component uses TCP port 5481 (default) to communicate to the ClearSCADA server and the server connects back to the client on TCP ports 5500-5509.

Make sure these ports are not being blocked on either machine hosting the OPC client or the ClearSCADA server. It is possible that your application might have different ports allocated for client-server communication.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: