Can the Altivar 312 drive be powered up with an external control voltage?
Issue:
External control voltage to power up an ATV312 drive.

Product Line:
ATV312

Environment:
All serial numbers for ATV312

Cause:
To program the drive with external voltage

Resolution:
No.  The VFD needs full supply voltage to power and program the drive.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: