Is it possible to fit reloading time by configuration / PLC Program of BMX EAE0300 ?
Question:
In the User Manual of Module BMX EAE0300,  you can find the following info:
Reloading Time  10 to 40 μs depending on encoder
Is it possible to fit reloading time by configuration / PLC Program?


Answer:
Actually, this is not the adjustable parameter for EAE module.
It is the requirement for the encoder spec to accommodate its communicate with the  EAE module.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: